Part Number: DS90UB940-Q1
我使用DS90UB940输出MIPI-DSI给SOC做视频输入,SOC再叠加其他图像后通过另外一个视频通道驱动TFT屏,有大约5%的产品无显示,但是把连接到940的视频线拔掉,再插上,就能显示了,这会是什么原因呢?
而另外约95%的产品一上电就正常的。这5%的故障产品,每次上电都无显示,插拔视频线后能恢复显示。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB940-Q1
我使用DS90UB940输出MIPI-DSI给SOC做视频输入,SOC再叠加其他图像后通过另外一个视频通道驱动TFT屏,有大约5%的产品无显示,但是把连接到940的视频线拔掉,再插上,就能显示了,这会是什么原因呢?
而另外约95%的产品一上电就正常的。这5%的故障产品,每次上电都无显示,插拔视频线后能恢复显示。
您好,5%的这部分,和95%的配置都是一样的吧? TFT屏和cable线都和正常显示的屏和cable交换验证了吗?
另外,这5%的器件和正常工作的器件是同一批次吗?您是在哪里购买的?
5%的这部分,和95%的配置都是一样的。
TFT屏和cable线都和正常显示的屏和cable交换验证了,故障是跟TI芯片走的,这个芯片装到好的PCB上,也会故障。好的芯片换到这个PCB上也会OK。
就是故障芯片装到那里,那里就会故障。
现在最新的发现是:有上述故障现象的装的芯片DS90UB940N-Q1,而DS90UB940-Q1是正常的。那么这个带N的与不带N的有啥区别呢?
您好,940和904N是完全可以P2P兼容和互相替代的,只是940N是940的升级版本。
新设计时,我们建议是用940N。
您好,您这边问题解决了吗?是否是使用940没问题,940N发生问题?
如果确实是这样的,我这边需要去确认一下,因为940N是940的升级版本,完全可以直接替换。
好的,我这边收到,确定是使用940没问题,但是940N是有问题的是吗?
另外, 还想和您确认下购买渠道,您是在哪儿购买的?