串行端使用的是DS90UB933接摄像头,帧率为40Hz,但是解串端输出的帧率只有一半即20Hz,可能有哪些原因?
936上有没有能够导出VS信号频率的方法呢?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
串行端使用的是DS90UB933接摄像头,帧率为40Hz,但是解串端输出的帧率只有一半即20Hz,可能有哪些原因?
936上有没有能够导出VS信号频率的方法呢?
Thanks!
您好,936的lock 引脚输出什么电平? 如果能正常lock,说明deseriazer能正确接收到serializer的数据并匹配MODE的设置。
另外,读取下936的寄存器0x73,0x74,0x75和0x76的值是否都正确?
检查下933的CSI-2 port的设置,比data lanes? 是否配置的continuous clock mode?