This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB962-Q1: 962是否支持4GBPS FPDLINK-III

Part Number: DS90UB962-Q1


我们目前使用960,外部REFCLK时钟25Mhz,采用4个720p环视摄像头,使用同步模式。

因为960缺货,因此想看看是否可以把960替换为962。目前看962规格书,发现标题说FPD-LINK最高支持3gbps,如何理解?FPDLINK=REFCLK*160,我们需要改晶振?

  • 您好,3Gbps"是区分"4G"器件和"3G"器件之间允许的 CSI-2吞吐量的一种方法。它实际上并不是指 FPD 通道本身的线速率(line rate)。960和962均采用4Gbps 正向通道运行、但962可支持每个输入端口高达2.528Gbps 的 CSI-2数据,而960可支持每个 CSI-2输入端口3.3Gbps 的吞吐量。962设计用于与935个串行器配对,具有小于2.528Gbps 的 CSI-2吞吐量、或与具有小于2.528Gbps 的 CSI-2吞吐量的953串行器。