This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDES954: 我的方案是否可行?

Part Number: TDES954
Other Parts Discussed in Thread: TSER953,

您好!我画了一个框图,使用咱们TDES954和TSER953,。
1)TDES954端与MCU(STM32)连接,作为整个系统I2C主。
2)TSER953端挂4个I2C设备,且这一端没有MCU。
3)TDES954和TSER953之间通过同轴线缆连接。
问题:
1)这种方案可行吗?
2)MCU控制TSER953端I2C从机设备有风险吗?
3)如果这种方案可以,可以描述下开发上的注意事项吗?
感谢!!
  • 您好,MCU是可以通过TDES954这边对TDES953进行控制的。但是953这边不能挂接4个I2C设备。

    参考数据手册7.5.1 I2C Interface Configuration。最多只能挂接2个I2C devices。所以挂接四个的话,应该是不可行的呢。