This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ds90ub947-q1 is used with DS90UB948-Q1, the pattern test is performed, and the screen is not displayed.
Perform the configuration according to 4.4 Cases in the SNLA132G document. Use the Without FPD-link III scheme and configure 948 to enter Pattern test. The screen displays no information and is backlit.
How should I judge the problem? Please give me a reply. Thank you very much
您好,
为更加有效地解决您的问题,我将您的问题发布在E2E英文技术论坛上了,将由资深的英文论坛工程师为您提供帮助,请耐心等待他们的回复:
To clarify, do you try to getting patgen to work on just the deserializer first before using patgen over the FPD-Link?
Could you share the script of the patgen registers setting? Also, please provide the specs for the display they are using as well.