Part Number: DS90UB941AS-Q1
since FPDLINK used NRZ coding, if the fpdlink rate is 2gbps, the upper frequency is 1GHZ,about the lower frequency, what is the lower frequency?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB941AS-Q1
since FPDLINK used NRZ coding, if the fpdlink rate is 2gbps, the upper frequency is 1GHZ,about the lower frequency, what is the lower frequency?
您好,为了方便沟通,我们直接用中文吧。
941的line rate范围为0.875~3.675Gbps/lane,即信号频率为0.4375~1.8375GHz/lane。
您这里指的upper或lower frequency具体指的是什么频率?是不是FPD link的line rate?即我所说的0.4375~1.8375GHz/lane?
最低不是0Hz,每个 PCLK 会把 24bit RGB 数据、控制信号、时钟信号编码成为 35bit 数据,而PCLK的频率范围single link为25Mhz~105Mhz,dual link模式下为50Mhz~210Mhz。line rate 和 PCLK 之间存在固定的 35 倍关系,Line rate= fPCLK *35。 所以可以计算得到line rate(min)=25*35=875Mbps, line rate(max)=3675Mbps.
您可以参考下这篇关于FPD link系列的器件速率介绍的应用手册: