This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB936-Q1: HSTXDBR Data bit rate的频率是否能微调?

Part Number: DS90UB936-Q1


在测试过程中,我们发现因为ISP端设备与DS90UB936链接使用时,只可采用模拟信号通讯,其中需要对消影区进行适配。在运行一段时间后,会出现画面整体往下缓慢循环平移的现象。

针对上述情况,我们想了解一下AC Electrical Characteristics CSI-2功能中,当外部采用了25MHz的晶振时钟,是否可以从软件方面对HSTXDBR Data bit rate的频率进行微调(936Mbps左右),以适配后端ISP设备。