Hi Kailyn Chen ,
请问948的哪个寄存器可以获取到视频信号的状态,就是能知道948是否有接收到芯片信号。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,可以通过RX_LOCK 这位来判断,您可以配置为0. 即只有当948接收到视频信号的时候才响应。
如果配置为1的话,即使没有视频信号,只要和serializer连接这位就响应。
所以按照您的应用需求,将其配置为1,然后再通过读取这个寄存器来确定是否有获取到视频信号。
这bit的意思是,RX_LOCK的条件,是当接收到有效的视频信号时lock,还是即使没有视频信号,但是当ser和des间的link建立好之后,就产生lock?
如果我们配置为0,比如正向通道应用,只有当ser端接收到有效的视频信号时,RX_lock才会响应,如果读取的值为1,那说明只是FPD link建立好,可能ser端并没有接收到有效的视频信号。