Part Number: DS90UB947-Q1
你好,如果DS90UB947的VDDIO接1.8V,是否可以通过DS90UB947的I2CSEL引脚悬空来选择DS90UB947的IIC电平为3.3V?还是此时IIC的电平只能是1.8V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB947-Q1
你好,如果DS90UB947的VDDIO接1.8V,是否可以通过DS90UB947的I2CSEL引脚悬空来选择DS90UB947的IIC电平为3.3V?还是此时IIC的电平只能是1.8V?
您好,只能是1.8V. I2C是参考VDDIO的,又因为VDDIO既可以是1.8V也可以是3.3V,所以通过I2CSEL 来选择是配置为1.8V还是3.3V两种选择。
如果VDDIO=3.3V的话,则I2CSEL则悬空。
你好,DS90UB947的VDDIO的电平手册中给出的是不可以选择的,只能使用1.8V电平,不具有可选性。

您好,不好意思,我记错了,948的VDDIO是既可以1.8V也可以是3.3V的。
947的VDDIO只能是1.8V。 但是如果I2CSEL悬空,则I2C的SDA和SCL也是需要上拉到3.3V的。

总之,如果I2CSEL上拉到VDDIO=1.8V,则I2C 需要上拉到1.8V。
如果I2CSEL悬空,则I2C需要上拉到3.3V。