Part Number: DS90UB913A-Q1
你好,请问下这款芯片的输入是数字视频DVP接口,一个像素时钟PCLK可以传输12或10位并行数据的一个像素点,也就是一个像素点最多只有12位数据,那这如何表示RGB或者YUV信息?难道每个像素点的RGB每种颜色只有三四位数据表示?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB913A-Q1
你好,请问下这款芯片的输入是数字视频DVP接口,一个像素时钟PCLK可以传输12或10位并行数据的一个像素点,也就是一个像素点最多只有12位数据,那这如何表示RGB或者YUV信息?难道每个像素点的RGB每种颜色只有三四位数据表示?
913的色深确实是12bit或10bit数据,主要针对YUV或RAW data或其他12bit或10bit的数据格式。
如果应用是RGB888或者RG666则推荐使用其他serializer。
你好,摄像头sensor的DVP接口输出的12位数据能直接接913么? 因为sensor每个PCLK输出的12位并行数据表示一个像素点,但是这个像素点可能都是单色的,这样可行么?
您好,sensor输出的12bit是什么数据格式?可能要看下913并行串行机制是否和数据格式一致,比如BT.656是不支持的,因为BT656指定了在数据的并行和串行格式之间进行的特定多项式扰频。DS90UB913A/914A 使用一个不同的扰频方案。