This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, as shown above, I think I know how to set DS90UB941AS-Q1? Realize the exchange of the display screen of the instrument and the central control, put the display screen of the instrument on the central control side, and the display screen of the central control on the instrument side, thank you
您好,按照您的这y个架构图,您的意思是想要实现仪表屏和中控屏的显示切换吗?
put the display screen of the instrument on the central control side, and the display screen of the central control on the instrument side
仪表屏在中控屏端,中控屏在仪表屏端,也就是实现这二者的切换是吗?
那触控屏在这里是不变的,也就是说要接三个屏是吗?
您好,抱歉,上面的UB941是1 lane输出接触摸屏,不用管它是吗?
下面的UB941,2 lane输出,接中控屏和仪表屏是吗?然后要实现中控屏和仪表屏的切换?
另外,UB941是串行LVDS 输出,这三个显示屏都是直接接UB941出来的FPD link信号是吗?
你好,系统款图如下,重点关注仪表屏和中控屏
上面的UB941是1 lane输出接触摸屏,不用管它是吗?
--> 是的, 上面的触摸屏不用管
下面的UB941,2 lane输出,接中控屏和仪表屏是吗?然后要实现中控屏和仪表屏的切换?
-->是的
另外,UB941是串行LVDS 输出,这三个显示屏都是直接接UB941出来的FPD link信号是吗?
--> 是的, 8155经过UB941出来后, 通过FPD link 直接到仪表屏和中控屏
我想知道如何设置UB941, 让仪表屏和中控屏的显示画面切换? 请支持一下, 谢谢.
您好,两个屏幕切换的话,意思就是对TX port0或TX port1的选择。 可通过寄存器0x1E TX_PORT_SEL 进行配置。