This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB964-Q1: 芯片的应用问题

Part Number: DS90UB964-Q1

关于TI的960和964,请问下Spec里面要求VDD和VDDIO的上升沿时间最小达到200ns,这个指标如果不满足的话会有什么负面影响?

还有一个问题,就是关于960和964的上电时序,不知道这个有没有明确的先后要求,看spec里,964写的是VDD11到VDD/VDDIO上电T0、T2、T4最小时间0ms,而且图例标的从电源稳定开始标的时间;但是960里写的是VDD/VDDIO到VDD11上电t最小时间0ms,但是图例标识从电源10%开始标的时间.

  • 请问下Spec里面要求VDD和VDDIO的上升沿时间最小达到200ns,这个指标如果不满足的话会有什么负面影响?

    首先合理的上电时序是保证芯片上电正常启动的前提,也是保证寄存器能正确读写的基础。

    如果没有按照这个要求的话,可能会导致输出的一些问题。

    关于上电时序,有上电时序要求的,需要按照datasheet中给出的时序。 对于您提到的delay标注,rise/fall time是按照10%~90%的范围。而delay时间则是稳定之后算。可能960的时序图中画的是有些偏差,但是t0是和964一样,需要从稳定开始标。