Part Number: DS90UB935-Q1
Dears,
请帮忙检查原理图设计,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
1.LPF2必须接0.1uF即100nF的电容到地,电路图中接的是C149为10nF。请改正。
2. LPF1这里接0.022uF=22nF电容到Pin11 VDD_PLL 没问题,然后我看您接了两个去耦电容,这里有个未接的GND。

3. SCL和SDA没看到上拉电阻,I2C是开漏输出,需要上拉。
4.PDB我看您这里直接接的1.8V和接GND,注意上电时PDB的时序即可。
其他没什么问题,另外935的原理图可以参考953的EVM user‘s guide中的原理图。