This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: Test pattern 在输出1280*720数据时异常。

Part Number: DS90UB960-Q1


在实际使用中,我们发现当输出1280*720p_yuv422_8bit@30fps的视频时,DS90UB960-Q1 总是多输出4列数据,总数据量为1284*720。

我们仅使用DS90UB960-Q1 测试模式输出时,发现仍然存在以上问题。

测试模式初始化代码如下:

0x32,0x01, //CSI0 select
0x33,0x03, //CSI_EN & CSI0 2Lane,BIT[5:4] controls lane count
0x21,0x83, // replicate port 0 to port 1
0x20,0x00, //e0//forwarding of RX0 to CSI0



0x1f,0x02,

0x4c,0x01,//
0x6E,0xAA, //BC_GPIO_CTL0: FrameSync signal to GPIO0/1
0x10,0x91,
0x58,0x58, //enable pass throu  BCC_CONFIG Register:BACK Channel config
		   
//0x19,0x01, //FS_HIGH_TIME_1
//0x1A,0x15, //FS_HIGH_TIME_0
//0x1B,0x09, //FS_LOW_TIME_1
//0x1C,0xc2, //FS_LOW_TIME_0
//0x18,0x01, //Enable FrameSync


//0x19,0x01, //FS_HIGH_TIME_1
0x1A,0x06, //FS_HIGH_TIME_0
0x1B,0x5b, //FS_LOW_TIME_1
0x1C,0x9b, //FS_LOW_TIME_0
0x18,0x43, //Enable FrameSync


//0x1f,0x02,

0x6d,0x7f, //Configure port to coax mode and FPD III to CSI mode
0x5c,0xb0, //7-bit Remote Serializer Alias ID 		TX_ID
0x5d,0x60, //7-bit Remote Slave Device ID 0 		Sensor ID
	//Sensor physical ID
	//Configures the physical I2C address of the remote I2C Slave device
	//attached to the remote Serializer. If an I2C transaction is addressed
	//to the Slave Alias ID3, the transaction is remapped to this address
	//before passing the transaction across the Bi-directional Control
	//Channel to the Serializer.
0x65,0x60, //7-bit Remote Slave Device Alias ID 0	Sensor Alias ID
	//Configures the decoder for detecting transactions designated for an
	//I2C Slave device attached to the remote Serializer. The transaction
	//is remapped to the address specified in the Slave ID0 register. A
	//value of 0 in this field disables access to the remote I2C Slave.
0x70,0x1e, //RAW10_datatype_yuv422b10_VC0

0x7c,0xe1,


0xB0,0x00,
0xB1,0x01,
0xB2,0x01,
0xB1,0x02,
0xB2,0x33,
0xB1,0x03,
0xB2,0x1e,//yuv8bit
0xB1,0x04,
0xB2,0x0a,//1280*2
0xB1,0x05,
0xB2,0x00,
0xB1,0x06,
0xB2,0x01,
0xB1,0x07,
0xB2,0xE0,
0xB1,0x08,
0xB2,0x02,
0xB1,0x09,
0xB2,0xD0,
0xB1,0x0A,
0xB2,0x04,
0xB1,0x0B,
0xB2,0x1A,
0xB1,0x0C,
0xB2,0x0C,
0xB1,0x0D,
0xB2,0x67,
0xB1,0x0E,
0xB2,0x21,
0xB1,0x0F,
0xB2,0x0A,

0x20,0x00, //e0//forwarding of RX0 to CSI0

如代码所示,我配置的测试模式输出为1280*720的yuv4228bit。但是我上位机软件必须要配置为1284*720去解析图像才能得到正确的图像,且图像右侧有明显的一列异常处,如下图所示。

/resized-image/__size/1920x1080/__key/communityserver-discussions-components-files/59/pastedimage1663579889886v1.png

如果我使用1280*720去解析,则得到图像如下图所示:

/resized-image/__size/1920x1080/__key/communityserver-discussions-components-files/59/pastedimage1663579947018v2.png

但是,有趣的是,我将test pattern 输出数据调整为1200x720 的yuv 输出,则并不会存在以上问题。代码改动如下:

0x32,0x01, //CSI0 select
0x33,0x03, //CSI_EN & CSI0 2Lane,BIT[5:4] controls lane count
0x21,0x83, // replicate port 0 to port 1
0x20,0x00, //e0//forwarding of RX0 to CSI0



0x1f,0x02,

0x4c,0x01,//
0x6E,0xAA, //BC_GPIO_CTL0: FrameSync signal to GPIO0/1
0x10,0x91,
0x58,0x58, //enable pass throu  BCC_CONFIG Register:BACK Channel config
		   
//0x19,0x01, //FS_HIGH_TIME_1
//0x1A,0x15, //FS_HIGH_TIME_0
//0x1B,0x09, //FS_LOW_TIME_1
//0x1C,0xc2, //FS_LOW_TIME_0
//0x18,0x01, //Enable FrameSync


//0x19,0x01, //FS_HIGH_TIME_1
0x1A,0x06, //FS_HIGH_TIME_0
0x1B,0x5b, //FS_LOW_TIME_1
0x1C,0x9b, //FS_LOW_TIME_0
0x18,0x43, //Enable FrameSync


//0x1f,0x02,

0x6d,0x7f, //Configure port to coax mode and FPD III to CSI mode
0x5c,0xb0, //7-bit Remote Serializer Alias ID 		TX_ID
0x5d,0x60, //7-bit Remote Slave Device ID 0 		Sensor ID
	//Sensor physical ID
	//Configures the physical I2C address of the remote I2C Slave device
	//attached to the remote Serializer. If an I2C transaction is addressed
	//to the Slave Alias ID3, the transaction is remapped to this address
	//before passing the transaction across the Bi-directional Control
	//Channel to the Serializer.
0x65,0x60, //7-bit Remote Slave Device Alias ID 0	Sensor Alias ID
	//Configures the decoder for detecting transactions designated for an
	//I2C Slave device attached to the remote Serializer. The transaction
	//is remapped to the address specified in the Slave ID0 register. A
	//value of 0 in this field disables access to the remote I2C Slave.
0x70,0x1e, //RAW10_datatype_yuv422b10_VC0

0x7c,0xe1,


0xB0,0x00,
0xB1,0x01,
0xB2,0x01,
0xB1,0x02,
0xB2,0x33,
0xB1,0x03,
0xB2,0x1e,//yuv8bit
0xB1,0x04,
0xB2,0x09,//1280*2
0xB1,0x05,
0xB2,0x60,
0xB1,0x06,
0xB2,0x01,
0xB1,0x07,
0xB2,0xE0,
0xB1,0x08,
0xB2,0x02,
0xB1,0x09,
0xB2,0xD0,
0xB1,0x0A,
0xB2,0x04,
0xB1,0x0B,
0xB2,0x1A,
0xB1,0x0C,
0xB2,0x0C,
0xB1,0x0D,
0xB2,0x67,
0xB1,0x0E,
0xB2,0x21,
0xB1,0x0F,
0xB2,0x0A,

0x20,0x00, //e0//forwarding of RX0 to CSI0

出图效果如下,图像右侧未见异常,且能按照设定的分辨率正常解析。

/resized-image/__size/1920x1080/__key/communityserver-discussions-components-files/59/pastedimage1663580221943v3.png

  • 您好,

    您可以提供所使用显示屏的active 和 blanking 参数吗?也请提供寄存器dump 以方便排查问题

  • 显示屏? 产品在开发阶段,现在是通过USB协议将视频数据上传到PC端显示的,所以跟显示屏没有关系。能确定的是: DS90UB960-Q1 CSI 端口发出的MIPI数据上,确实比预期的1280*720 要多 4*720 的数据量。   另外请问寄存器dump 是需要将0x00 -0xff 的寄存器值都读出吗?如果是的话测试模式test pattern 下DS90UB960-Q1 的寄存器值如下:

    0x0,0x7a,
    0x1,0x00,
    0x2,0x1e,
    0x3,0x40,
    0x4,0xd0,
    0x5,0x01,
    0x6,0x00,
    0x7,0xfe,
    0x8,0x1c,
    0x9,0x10,
    0xa,0x7a,
    0xb,0x7a,
    0xc,0x0f,
    0xd,0x09,
    0xe,0x01,
    0xf,0xff,
    0x10,0x91,
    0x11,0x00,
    0x12,0x00,
    0x13,0x00,
    0x14,0x00,
    0x15,0x00,
    0x16,0x00,
    0x17,0x00,
    0x18,0x43,
    0x19,0x00,
    0x1a,0x06,
    0x1b,0x5b,
    0x1c,0x9b,
    0x1d,0x00,
    0x1e,0x04,
    0x1f,0x02,
    0x20,0x00,
    0x21,0x83,
    0x22,0x00,
    0x23,0x00,
    0x24,0x00,
    0x25,0x00,
    0x26,0x00,
    0x27,0x00,
    0x28,0x00,
    0x29,0x00,
    0x2a,0x00,
    0x2b,0x00,
    0x2c,0x00,
    0x2d,0x00,
    0x2e,0x00,
    0x2f,0x00,
    0x30,0x00,
    0x31,0x00,
    0x32,0x01,
    0x33,0x03,
    0x34,0x00,
    0x35,0x01,
    0x36,0x00,
    0x37,0x01,
    0x38,0x00,
    0x39,0x00,
    0x3a,0x00,
    0x3b,0x00,
    0x3c,0x00,
    0x3d,0x00,
    0x3e,0x00,
    0x3f,0x00,
    0x40,0x00,
    0x41,0xa9,
    0x42,0x71,
    0x43,0x01,
    0x44,0x00,
    0x45,0x00,
    0x46,0x20,
    0x47,0x00,
    0x48,0x00,
    0x49,0x00,
    0x4a,0x00,
    0x4b,0x12,
    0x4c,0x01,
    0x4d,0x13,
    0x4e,0x04,
    0x4f,0x1a,
    0x50,0x13,
    0x51,0x00,
    0x52,0x00,
    0x53,0x00,
    0x54,0x00,
    0x55,0x00,
    0x56,0x00,
    0x57,0x00,
    0x58,0x58,
    0x59,0x00,
    0x5a,0x00,
    0x5b,0xb2,
    0x5c,0xb0,
    0x5d,0x60,
    0x5e,0x00,
    0x5f,0x00,
    0x60,0x00,
    0x61,0x00,
    0x62,0x00,
    0x63,0x00,
    0x64,0x00,
    0x65,0x60,
    0x66,0x00,
    0x67,0x00,
    0x68,0x00,
    0x69,0x00,
    0x6a,0x00,
    0x6b,0x00,
    0x6c,0x00,
    0x6d,0x7f,
    0x6e,0xaa,
    0x6f,0x88,
    0x70,0x1e,
    0x71,0x2c,
    0x72,0xe4,
    0x73,0x00,
    0x74,0x00,
    0x75,0x00,
    0x76,0x00,
    0x77,0xc5,
    0x78,0x00,
    0x79,0x01,
    0x7a,0x00,
    0x7b,0x00,
    0x7c,0xe1,
    0x7d,0x00,
    0x7e,0x00,
    0x7f,0x00,
    0x80,0x00,
    0x81,0x00,
    0x82,0x00,
    0x83,0x00,
    0x84,0x00,
    0x85,0x00,
    0x86,0x00,
    0x87,0x00,
    0x88,0x00,
    0x89,0x00,
    0x8a,0x00,
    0x8b,0x00,
    0x8c,0x00,
    0x8d,0x00,
    0x8e,0x00,
    0x8f,0x00,
    0x90,0x00,
    0x91,0x00,
    0x92,0x00,
    0x93,0x00,
    0x94,0x00,
    0x95,0x00,
    0x96,0x00,
    0x97,0x00,
    0x98,0x00,
    0x99,0x00,
    0x9a,0x00,
    0x9b,0x00,
    0x9c,0x00,
    0x9d,0x00,
    0x9e,0x00,
    0x9f,0x00,
    0xa0,0x00,
    0xa1,0x00,
    0xa2,0x00,
    0xa3,0x00,
    0xa4,0x00,
    0xa5,0x1a,
    0xa6,0x00,
    0xa7,0x00,
    0xa8,0x00,
    0xa9,0x00,
    0xaa,0x00,
    0xab,0x00,
    0xac,0x00,
    0xad,0x00,
    0xae,0x00,
    0xaf,0x00,
    0xb0,0x00,
    0xb1,0x0f,
    0xb2,0x0a,
    0xb3,0x08,
    0xb4,0x25,
    0xb5,0x00,
    0xb6,0x18,
    0xb7,0x00,
    0xb8,0xfb,
    0xb9,0x33,
    0xba,0x83,
    0xbb,0x74,
    0xbc,0x80,
    0xbd,0x00,
    0xbe,0x00,
    0xbf,0x00,
    0xc0,0x00,
    0xc1,0x00,
    0xc2,0x00,
    0xc3,0x00,
    0xc4,0x00,
    0xc5,0x00,
    0xc6,0x00,
    0xc7,0x00,
    0xc8,0x00,
    0xc9,0x00,
    0xca,0x00,
    0xcb,0x00,
    0xcc,0x00,
    0xcd,0x00,
    0xce,0x00,
    0xcf,0x00,
    0xd0,0x00,
    0xd1,0x43,
    0xd2,0x94,
    0xd3,0x02,
    0xd4,0x60,
    0xd5,0xf2,
    0xd6,0x00,
    0xd7,0x02,
    0xd8,0x00,
    0xd9,0x00,
    0xda,0x00,
    0xdb,0x00,
    0xdc,0x00,
    0xdd,0x00,
    0xde,0x00,
    0xdf,0x00,
    0xe0,0x00,
    0xe1,0x00,
    0xe2,0x00,
    0xe3,0x00,
    0xe4,0x00,
    0xe5,0x00,
    0xe6,0x00,
    0xe7,0x00,
    0xe8,0x00,
    0xe9,0x00,
    0xea,0x00,
    0xeb,0x00,
    0xec,0x00,
    0xed,0x00,
    0xee,0x00,
    0xef,0x00,
    0xf0,0x5f,
    0xf1,0x55,
    0xf2,0x42,
    0xf3,0x39,
    0xf4,0x36,
    0xf5,0x30,
    0xf6,0x00,
    0xf7,0x00,
    0xf8,0x00,
    0xf9,0x00,
    0xfa,0x00,
    0xfb,0x00,
    0xfc,0x00,
    0xfd,0x00,
    0xfe,0x00,
    0xff,0x00,
    

  • 为更加有效地解决您的问题,我将您的问题发布在了E2E英文技术论坛上,将由资深的英文论坛工程师为您提供帮助,请耐心等待回复:

    https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1136137/ds90ub960-q1-abnormal-when-output-1280-720-in-test-pattern-mode