This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: DP83867电源供电问题。

Part Number: DP83867IR


DP83867IRPAP采用双电源供电,IO电压为3.3V,VDDA2P5和VDD1P1供电电压在DCDC端正常。经过磁珠进入PHY芯片后,2V5变成3.14V左右。断开磁珠后,磁珠前级DCDC也是2V5, 磁珠后级PHY端依然有3.14V左右的电压。

DEBUG手段:

1. 取下芯片后,磁珠前后级都是2v5。

2. 因为是配置为advertise ablility of 10/100/1000,  aneg_sel0和aneg_sel1都为0,MODE1为上下拉OPEN.Rb

3.RBIAS确认是11K±1%精度。

请问还有其他原因导致这样的问题吗?