This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB633A-Q1: If DS90UB633A-Q1 support 2M/30fps Camera

Part Number: DS90UB633A-Q1
Other Parts Discussed in Thread: DS90UB662-Q1, DS90UB933-Q1

Hi,

Two questions: 

1) If DS90UB633A-Q1 support 2M/30fps Camera?  

2) If DS90UB662 could be compatible with 933? 

3) Could the VOUT Interface of 24-bit parallel, 1080p@60fps connect to 633?

Thanks a lot! 

Andy 

 

  • 1.  2M/30fps is 1600*1280@30fps。Take 15% blanking time for example:

    Let's calculate the pixel clock=1600*1280*30*(1+15%)=70.656Mhz。

    While UB633A support 56.25-MHz to 100-MHz input pixel clock。 So 2M/30fps could be no problem.

    2.The 6xx parts are a part of our  low cost roadmap and will not be compatible with the existing 9xx parts.  So the DS90UB933-Q1 part is not compatible with the DS90UB662-Q1 part。

    3. The DIN is [11:0]. So it could support 10bit or 12bit. So 24-bit parallel couldn't support.