This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1210: CPEN,VBUS,ID三者的关系,及如何验证,可否使用UART操作寄存器

Part Number: TUSB1210


我想验证一下TUSB1210是否工作正常,但是我没有接主芯片,不知是否可以通过UART验证

不接主芯片的话,CPEN,VBUS实际输出是低电平,

手册中提到CPEN需要把DRVVBUS和DRVVBUSEXTERNAL这俩寄存器置1才可以输出高电平,要怎么操作呢?可以通过UART操作吗

  • TUSB1210是否工作正常,但是我没有接主芯片,不知是否可以通过UART验证

    硬件的话看下电源,输入时钟,REST等这些引脚是否正常。

    手册中提到CPEN需要把DRVVBUS和DRVVBUSEXTERNAL这俩寄存器置1才可以输出高电平,要怎么操作呢?可以通过UART操作吗

    不可以,只能通过 ULPI 并行接口通过寄存器写入来设置DRVBUS和DRVBUSSEXTERNAL配置为UARTmode。