This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: 芯片的带宽问题

Part Number: DS90UB953-Q1


我们现在用DS90UB953,Spec有个疑问,这里CSI总的带宽最大f*64,但是我们现在CSI只用了1lane,如果我们输入参考时钟用25MHz的话,CSI最大带宽就是1600,这个需要除以4折算到每个lane上吗

  • 参考下面表格,f*64 是针对非同步模式的。 CSI带宽是由lane的数量以及each lane能够支持的最大data rate决定的。

    所以当25Mhz参考时钟,f*64=1200Mbps是4lane总的带宽。 所以each lane能够支持的data rate为300Mbps.

    同样 ,同步模式下,总带宽小于f*128。以26Mhz为例,总带宽为3.328Gbps,这是4lane总的带宽,那么each lane支持的data rate为832Mbps,即datasheet首页介绍的: