如果953芯片连接的LVDS cable对电源和地短路或者断路,953是否的寄存器是否可以检测到这种情况?
如果不能检测到的话,后端的960芯片是否可以支持?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,FPD link器件好像是没有电源短路的保护模块。
960也没有专门寄存器针对cable的问题或者电源对地短路的监测。
但是960的0x4D bit1和bit0 ,比如我们可以通过读取这两位来判断960的RX是否已经对953的输出数据已经锁存,RX是否满足pass的标准,如果这两位都不满足的话,那么在debug的过程中就可以去更换cable是不是cable的连接有问题。