This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS250DF810: DS250DF810ABVT

Part Number: DS250DF810
Other Parts Discussed in Thread: DS125DF410

芯片手册描述支持20.2752至25.8Gbps的速率,包括10.3125Gbps、12.5Gbps等子速率。 是否可以应用到25G的CPRI接口和10G 的CPRI接口 (是否支持10.1376Gbps和9.8304Gbps等速率)?

如果不支持,是否有推荐型号?

x 出现错误。请重试或与管理员联系。