This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Support Team
我們客戶 目前 功能架構如下, 對於TX跟RX端的Redrive都放在USB-C Board, 在設計上 有需要注意的地方嗎?
if any, Please advise me.
Thanks,
Best regards,
Lawrence
您好,IVI board和USB-C board之间的距离很长吗?
另外USB3.2 GEN MUX距离connnector的距离有多远?您是采用的USB3.2的MUX是吗?另外注意TUSB501支持到USB3.0 的。
对于TUSB501来说,它具有transmitter的de-emphasis又具有receiver端的均衡处理,从您的应用架构来看,您采用它的主要目的是利用recevier的均衡处理对吧?我看它是靠近MUX的。
Hi, Kailyn
目前客戶選用USB3.2 MUX HD3SS3212-Q1 , Redrive 是選用 TUSB501-Q1
由於電纜太長(~1m), 所以在加redrive, 但您剛有提到 TUSB501-Q1 只有支持到5Gbps.
請問有10Gbps 解決方案 + HD3SS212-Q1?
就我所理解 HD3SS3212-Q1 + TUSB501-Q1 最高只支持到5Gbps 對吧?
if any, Please advise me.
Thanks,
Best regards,
Lawrence
是的,因为TUSB502只能支持到5Gbps的速率,即使 HD3SS3212能支持到10Gbps,但是和TUSB502 搭配使用的话,那么限制了速率只能到5Gbps。
下面是我筛选出来USB redriver 支持10Gbps的几款器件,但是我看您使用的都是汽车级,所以不知道是否满足您的应用需求。