XIO2001的PCI复位信号一直在复位,上机后主机能找到XIO2001设备,但是XIO2001无法找到后端的PCI设备,经排查33Mhz时钟信号波形正常,但始终无法使PCI复位信号拉高,完成复位!接下来我该怎么排查??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
请注意,当GRST置低电平的时候PRST也会置低,当 bridge control 寄存器(3Eh ) Bit 6 (SRST)置 1时,PRST 也会置低,具体见 8.4.30章节。
有人发现PCIe TX和RX信号的线连接错误会造成这种现象,请检查PCIe TX和RX信号线的连接:
也有人发现GND焊接不良会造成这种现象,您测试几块设备是这种现象?请多测试几块以排除焊接问题: