DP83620接入了一个25M的晶体,但是测试无输出,需要哪些配置?请各位指教!谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢,问题已解决!
但是怎么配置才能让MII_TX_CLK和MII_RX_CLK输出25M的时钟?
另外想问一下,如果用AM3352的GMII接口,是不是只能配置成GMII接口?
只要DP83620工作在MII 100M模式,这两个脚就会是25M。
DP83620属于100M的PHY,是不支持GMII接口的。
不是的,我看了下AM3352,它还支持MII和RMII接口,这些可以和DP83620对接。