TI 工程师
你好
有个问题请教下,我们现在有个项目在使用DS90UB948,在使用的时候发现,当PDB引脚拉高后,LVDS就会输出一个1.2V的直流电平(如下图),这个直流电平会串电给LCD里面在芯片,从而导致有时会出现显示异常,948有办法控制LVDS输出吗(通过I2C控制,;LVDS信号需要输出在时候才输出)。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI 工程师
你好
有个问题请教下,我们现在有个项目在使用DS90UB948,在使用的时候发现,当PDB引脚拉高后,LVDS就会输出一个1.2V的直流电平(如下图),这个直流电平会串电给LCD里面在芯片,从而导致有时会出现显示异常,948有办法控制LVDS输出吗(通过I2C控制,;LVDS信号需要输出在时候才输出)。
您好,两个问题和您确认:
第一,就是948的上电时序以及PDB pin是不是符合datasheet中的上电时序要求?

第二,948的输入端和前端serilaizer的输出连接的时候,有没有加AC耦合电容?

1.2V是LVDS的共模电压,差分输出的话 ,这个共模会被抑制掉了。
您这个波形是单端输出测试的对吧?那应该是正常的呢。当PDB拉高,器件进入正常操作,单端LVDS输出是以1.2V为参考电压的。
Hi Kailyn Chen
如果948的LVDS 1.2V共模电压先输出,就会串电到LCD的3.3V上面,还有个问题请教下,怎么让948的输出MUTE掉,就是不输出LVDS信号,可以有1.2V共模电压输出。谢谢
参考Table 7-1.将0x02 bit7=L,bit4=1,输出高阻态试试。