This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90CP04: 通信接口设计咨询

Part Number: DS90CP04


您好,请教几个关于DS90CP04的设计问题:

1.按照SPEC的要求,我的理解连接方式如图。请帮忙确认RSO和CSO是否连接正确,是否出现在合适的行或者列的位置上。

2.如果要读出指定DS90CP04的寄存器值,是要把每一行的最后一个设备的RSO和RSCLK引出来接入到Host里?需要将最后一个设备的CSO引出来吗?(上图红色部分)

3.按照你们的观察,读出的连接接口是否有必要引出来,因为我们的row数量比较多。资源也有限。

4.下方的图片我没太理解,请帮忙解释:

4.1ConfigA和ConfigB是同一个设备里两个配置吗?理论上一个设备不是只有一个配置在Load里面等待加载吗?我理解是:比如在NxN的矩阵中,依次对所有设备都写一次配置到load 寄存器中。下图中的那A和B其实就是一样的?第二个load上升沿纯粹是为了打开OUT,但两次加载的load寄存器内容其实是一样的?

4.2LOAD在L->H->L->H的过程中,除了OUT对LOAD高电平持续时间有约束(tsw,toff,ton)。是否对LOAD信号的高电平持续的最大时间有要求?以及两个高电平之间的低电平是否有最大和最小时间的要求?因为我们想用一个低速普通的IO去控制这个信号,所以LOAD的频率不会太高。

4.3LOAD拉高的时间只要在配置写入完成之后就可以吗,不管啥时候?

5.在交换矩阵中,前级DS90CP04和下一级的DS90CP04连接,是否还需要为LVDS加100R端接电阻?