This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教用这种CAN隔离器与别的CAN设备通信的时候 这两个设备之间需要共地吗?
CAN传的是差分信号,不需要共地。
而且系统间是通过总线链接的,你没法做地线链接。
ISO1050左端设备的GND和GND1共地,右端的GND和GND2共地,通过ISO1050隔离,不会产生地回流。
也就是说,右边的GND2是需要连线到右边设备的GND去的,左边的GND1需要连线到左边设备的GND?
是的啊
右边的GND2是需要连线到右边设备的GND去,左边的GND1需要连线到左边设备的GND,互不干扰,这是隔离的意义