TI933摄像头YUV422数据用12bit输出,TI954设置Raw12格式,乱码。
请问raw12 mode有raw10 mode 的RAW10_8BIT_CTL方法吗?
TI933配置:
0x05,0x22, //12bit mode
TI954配置:
0x6d,0x7e, // RAW12 Mode

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI933摄像头YUV422数据用12bit输出,TI954设置Raw12格式,乱码。
请问raw12 mode有raw10 mode 的RAW10_8BIT_CTL方法吗?
TI933配置:
0x05,0x22, //12bit mode
TI954配置:
0x6d,0x7e, // RAW12 Mode

954 除了0x6D配置为RAW 12 bit 模式之外,0x71也要配置为0x2C RAW12 bit mode。
看下目前0x71是否配置的0x2C ,不是的话,配置成0x2C试试还是乱码吗?
另外,954的电路上IDX的上下拉电阻的配置是否也是12bit mode?参考Table2的strap 配置。
这个mode能上电后通过寄存器override吗?
可以的。上电后这个寄存器默认的是Table 2 MODE引脚上下拉阻值对应的模式,如果修改此寄存器,可以override strap pin。
抱歉,回复晚了,954的RAW12 mode确实没有raw10 mode 的RAW10_8BIT_CTL方法。
954设置成RAW12 mode,乱码,您设置的是RAW 12LF还是HF?像素时钟低于50Mhz建议配置为LF模式。
另外我也需要再看下这个问题,不好意思。
那您读取下状态寄存器0x4D的值,看是否有报错 ,以及bit0和bit1的值,看953是否有效接收到serializer输出的数据,是否符合pass标准。