This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947-Q1: DS90UB947-Q1

Part Number: DS90UB947-Q1

1、DS90UB947-Q1串行器贴片PCBA后组装成导航总成,通电检查在倒车360影像模式下目视观察屏幕上有花屏问题(雪花飘闪,见附件视频)

2、与OpenLDI解串器器SMD/DS90UB948TNKDRQ1/WQFN64/-40~105℃ 配合使用;有花屏总成检查零件线路波形、阻抗正常;VDDIO电压1.8V;

交叉验证:

3、将有花屏总成上芯片更换到无花屏总成上,花屏问题存在;将无花屏总成上芯片更换到有花屏总成上花屏问题消失;花屏问题随芯片;

4、失效产品(芯片)检测环境温度:约24℃-28℃;

5、失效产品(芯片)表面丝印:UB947Q TI22I C4LD G4、UB947Q TI22I C1ER G4、UB947Q TI22I AP42 G4(供参考);

6、断电后再次通电失效现象未解除;

  • 您好,雪花视频没有附上哈。

    我想问下,您是在哪儿购买的芯片?是在TI 网上商城吗?

    失效芯片当出现雪花时,948输出lock引脚为什么电平?可以读取下状态寄存器看是否有error报错? 

x 出现错误。请重试或与管理员联系。