Part Number: XIO2001
Windows10系统能够识别出来XIO2001及下端的CPCI串口板卡,windows系统设备管理器里面能够识别出来串口板卡的COM口,但是从系统COM口收发数据串口卡无输出(串口卡在其他CPCI主机上面测试没问题)。
请问XIO2001使用前是否需要进行配置或者要在EEPROM烧写配置文件吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: XIO2001
Windows10系统能够识别出来XIO2001及下端的CPCI串口板卡,windows系统设备管理器里面能够识别出来串口板卡的COM口,但是从系统COM口收发数据串口卡无输出(串口卡在其他CPCI主机上面测试没问题)。
请问XIO2001使用前是否需要进行配置或者要在EEPROM烧写配置文件吗?
不 进行配置或者不使用EEPROM就使用XIO2001的默认配置。

如果需要配置不是默认值时,那是需要使用EEPROM,参考上述手册中的描述,如果外部EEPROM不使用的话,将SCL下拉电阻到GND。
谢谢解答!
根据您的意见将SCL接10K电阻下拉到地,问题还是没有解决。请教下系统能够识别PCI设备,也能打开PCI设备的串口,但是通过系统识别出来的串口收发数据设备端COM却没有信号,这可能会哪那方面有关系呢?示波器测量FRAM TRDY IRTY DEVSEL信号上电后及打开关闭串口过程中均有拉低的脉冲。
您好,您参考下面这个帖子,也是通信不正常的例子,您看下是否对您有所帮助: