Other Parts Discussed in Thread: ISO1050
ti网站中,在使用iso1050的应用举例里,rtn接线端子接大地吗?还是哪里?怎么处理iso1050副边的地?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ISO1050
ti网站中,在使用iso1050的应用举例里,rtn接线端子接大地吗?还是哪里?怎么处理iso1050副边的地?
Hi Yingzhi,
ISO1050是隔离CAN收发器,顾名思义,其目的就是把CAN的逻辑端和总线端进行隔离,此时,两边的GND1和GND2可以容忍最大5000KV rms (DW pakcage)的电压差。对于你的问题,若CAN总线侧(右边)接TVS,此时把TVS的GND接ISO1050右边的GND2。下面是一个例子供你参考:focus.ti.com/.../getliterature.tsp
希望上面的答复能帮到你,谢谢!
Steven
ti公司的各位技术人员,我的问题是例子种的rtn接线端子接副边地的同时是否接大地?很感谢回复我,只是没有回复我的问题。
Dear Yingzhi,
前面跟你介绍了ISO1050的工作原理。从器件的工作原理角度看,以及上面提到的例子(参考:focus.ti.com/.../getliterature.tsp),RTN是可以直接接GND2的!
至于是否可以 接GND,关键看你系统是如何进行隔离了!就如从器件的工作原理看,GND1和GND2可以隔离5000V,若右边是你本地的GND,而左边的GND1跟你本地的GND要进行隔离,同时压差在5000V以内,则可以被GND2和你本地的GND相连!
HI:
您好,我对于该文档中,此公式:RF × CF = 0.032 / fS 中0.32是怎么确定的很感兴趣。请问这个公式怎么来的?