显示屏2880 x 1800 eDP 解串器TI984
使用TI哪款串行器可以通过HDMI转成FPD LINK
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,非NDA器件HDMI输入,FPD link输出的像DS90UB949不支持这么高分辨率呢。
NDA器件的话,我这边需要去确认。然后因为NDA器件不能在公共论坛上讨论,所以我这边会私信给您。
您好,2880 x 1800的分辨率,帧率frame rate是多少?按照15%的消隐来算,949能够支持的像素时钟为170Mhz。
那么170=2880 x 1800*frame rate*(1+15%)
这样计算出来最大frame rate为28fps。
也就是说如果2880 x 1800@30hz或2880 x 1800@60hz的分辨率,NDA器件或者非NDA都没有满足要求的。
但是如果帧率小于28fps,DS90UB949可以考虑和984搭配使用。
DS90UH984是能够支持2880 x 1800@60hz,并且输出eDP。
但是HDMI输入的Serializer,目前还没有能支持这么高分辨率的Serializer。
其他能支持这么高分辨率的串行器,DS90UB983是可以的,但是它的输入是DP,不是HDMI。
您好,983因为是NDA器件,需要我这边去美国工程师要申请的链接,如果您这边需要,我们私信聊983的问题。