This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB935-Q1: 串行器935解串器UB954与sensor芯片OX01F10的配置问题

Part Number: DS90UB935-Q1
Other Parts Discussed in Thread: DS90UB954-Q1,

目前模组由UB935与sensor芯片OX01F10组成。其中935与01F10是用2-lane的mipi信号,数据类型为raw;935与954是YUV422。请问一下935配置有哪些需要注意的地方,请说明一下?935的工作模式为Synchronous,目前的配置文件能之别芯片的I2C地址,但是不能出图,以下是配置参数

//TI935
0xfff8,0x30,
0xffff,0x64,

0x01,0x03,
0x02,0x53, //2lane Continous CLK

//I2C MODE
//0x0b,0x13,
//0x0c,0x26,
0x0b,0x7F,
0x0c,0x81,


//GPIO3 pulleUp Pwdn; GPIO0 as for Fysnc
0x0e,0x81,//GPIO_0/1 output enable 30
0x0d,0x18,//GPIO_0/1 01 03
//0x0d,0x0c,


//0x0e,0xc3,
//0x39,0x6c,
//0x41,0x6c,
0x39,0x00,
0x41,0x00,

0x33,0x23,
0x4c,0x01,
0x20,0x08,
//0x58,0x7a,
0x58,0x7e,
0x7c,0x81,


//24M MCLK output

0x07,0x7d //7d
0x06,0x63 //63


0xfff8,0x60
0xffff,0x0a
//0x58,0x5e

  • 您好,我们已收到您的问题并升级到英文论坛寻求帮助。由于国外假期,回复将会有所延迟(直至1月4日),感谢您的耐心等待!

  • 您好,

    其中935与01F10是用2-lane的mipi信号,数据类型为raw;935与954是YUV422

    能麻烦再解释一下吗?没太理解您的意思。DS90UB935-Q1和 DS90UB954-Q1会在收到时通过 CSI-2数据包。 不会调整视频的数据类型。 因此如果传感器向935提供raw视频,954也会输raw数据包。 

    935的工作模式为Synchronous,目前的配置文件能之别芯片的I2C地址,但是不能出图

    这句话也没太理解,能否麻烦再阐述一下?

  • 意思是我935配置的是YUV422输出,但是传感器向935提供raw视频;

    关于I2C我是通过954可以读取到935的slave id和sensor的slave id ,但是没有图像
  • 您好,

    935中没有任何函数可以让串行器将输入raw视频转换为 YUV422或任何其他格式。 所以我们还是很困惑您在这里做的操作。