你好!
我把LMH0302接到FPGA的高速收发器上,然后通过一根线缆连接到SDI显示器。fpga发送SDI数据后,显示器没有检测到输入视频。我的设计中只使用了一个LMH0302,没有使用reclocker。请问LMH0302与FPGA之间是否需要再加一个reclocker?我测试的视频规格是720p@60和1080p@60
以下是我的SDI原理图,其中CD1_SD_nHD为低,CD1_ENABLE为高

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
我把LMH0302接到FPGA的高速收发器上,然后通过一根线缆连接到SDI显示器。fpga发送SDI数据后,显示器没有检测到输入视频。我的设计中只使用了一个LMH0302,没有使用reclocker。请问LMH0302与FPGA之间是否需要再加一个reclocker?我测试的视频规格是720p@60和1080p@60
以下是我的SDI原理图,其中CD1_SD_nHD为低,CD1_ENABLE为高

您好,reclocker的目的是对clock信号的jitter的去除,提供更好的时钟信号完整性。
The reclocker attenuates high frequency jitter and provides the best signal integrity. High input jitter tolerance of the reclocker improves timing margin。
按照您的描述,目的是为了延长cable,添加cable redriver来补偿cable带来的损耗。 所以我想不需要加reclocker。
现在显示器不显示,去掉cable的话,直接FPGA接显示器是否能显示?