This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD2EUSB30A: the difference with TPD2EUSB30DRTR?

Part Number: TPD2EUSB30A


TPD2EUSB30ADRTR:3.6V
TPD2EUSB30DRTR:5.5V

so which one is better for ESD and surge test?

  • 您好,

    它们的ESD性能是一样的,它们的区别是工作电压Vrwm 和击穿电压VBR不同,带'A'的Vrwm (3.6V对5.5V)和VBR (4.5V对7V)略低。

    将带"A"器件(3.6 V)替换为不带"A"的(5.5 V)会更容易,因为切换至更高的Vrwm不会影响正常工作。如果将不带"A"的器件换为带"A"器件,则可能会出现问题。

    我们建议是对5 V线路使用不带“A”的器件,对3.3 V线路使用带“A”的器件。

  • 我们目前对与电脑连接的USB 5V线路具体使用了TPD2EUSB30ADRTR:3.6V。

    大批量运行了1~2年暂时没有问题。

    这样看来TPD2EUSB30ADRTR更换为TPD2EUSB30DRTR也是可以的。

    非常感谢回复。