Other Parts Discussed in Thread: SN74ACT244
您好:
我们的硬件中有一块是FPGA的的输出口接缓冲芯片送出TTL信号。FPGA的输出端是LVCMOS33,高电平3.3V。低电平0V。
由于所需要的输出驱动电流及芯片封装大小的需求,我们使用了两种接口缓冲芯片,SN74ACT244和SN74AS1034。
在实际使用中发现:FPGA上电后有一个500ms的配置过程,在此期间,FPGA的IO口为高阻态,但是在这时候,FPGA和SN74AS1034相连的引脚上的电压却为3.3V,和SN74ACT244相连的引脚上的电压为0V。
由于PCB面积限制苛刻,可能做不到为SN74ACT244所有的接口缓冲芯片的输入端都接上拉和下拉电阻(SN74AS1034管较少可以),所以我的问题是,像这类接口缓冲芯片的内部结构是什么样的,如果输入端为高阻态,输出端是否可以当做是稳定的高电平或低电平呢。
谢谢!