This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI有哪款料号可以代替ISL90726UIE627Z-TK

TI有哪款料号可以代替ISL90726UIE627Z-TK ??

 

    • Volatile Solid-State Potentiometer
    • I2C Serial Bus Interface
    • DCP Terminal Voltage, 2.7V to 5.5V
    • Low Tempco
    • Rheostat - 45 ppm/°C typical
    • Divider - 15 ppm/°C typical
  • 128 Wiper Tap Points
  • Wiper Resistance 70Ω typ at VCC = 3.3V
  • Low Power CMOS
  • Active Current, 200µA Max
  • Standby Current, 500nA Max
  • Available RTOTAL Values = 50kΩ, 10kΩ
  • Power on Preset to Midscale
  • Packaging
  • 6 Ld SC-70
  • Pb-Free (RoHS compliant)