This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE706

Other Parts Discussed in Thread: CDCE706

需要在byte10中设置 S00,S01,S10,S11 为 1 , A0,A1 pin 才可以作为 地址 使用, 这个设置是如何进行的(设置时地址没有确定,如何知道是设置哪个CDCE706 slvae)?

急盼回复,谢谢

  • Hi Yingqi,

    CDCE706默认的I2C地址是1101001,故若有多片CDCE706挂在同一个I2C总线上,则刚开始第一次写操作就是要把所有CDCE706(总共可以挂4pcs的CDCE706)BYTE10的S0/S1更改为A0A1的含义,然后在再一个读写周期,就可以按各自的I2C地址读写。

    Steven

x 出现错误。请重试或与管理员联系。