This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TTL转LVDS-LVDS转TTL后,液晶屏显示抖动的问题

Other Parts Discussed in Thread: DS90CF386

项目要求将ARM的LCD输出RGB的TTL电平转为LVDS,再将LVDS转换为液晶屏的TTL电平,使用LVDS接口传输数据达到降低液晶屏线上辐射的目的。

我们将DS90C385和DS90CF386成对使用。DS90C385将TTL转为LVDS,DS90CF386再将LVDS转换为TTL,供液晶RGB和控制使用。RGB使用的格式的656,好像两个芯片都支持656的格式。

现在的问题是显示静态图片时芯片和图像各个参数正常;而程序动态刷新显示区时图像抖动,测试发现控制信号中的帧同步信号的VFRAME输出的36HZ不正常。静态图片时VFRAME输出为36HZ的脉冲信号,而动态刷新显示区时在VFRAME的36HZ脉冲上出现了很多随机的脉冲,此时ARM输出的VFRAME为正常的36HZ的脉冲信号,而DS90CF386的输出就出现了很多随机的脉冲,导致图像不稳定,测试时发现在其他控制信号上也有干扰脉冲的现象。

现在基本排除是ARM输出的问题,主要问题还是集中在DS90C385和DS90CF386的转换电路上。

DS90C385使用上升沿取数,LVDS和PLL供电都使用磁珠和3.3V隔开,并加入多种大小的去耦电容,LVDS和PLL的地线都使用零欧姆单点接地;DS90CF386的电和地的处理与DS90C385一致。

 

 

x 出现错误。请重试或与管理员联系。