Other Parts Discussed in Thread: TXB0108
请问TXB0108的datasheet上说没有用到的IO要接GND或电源,如下:The A and B sides of an unused data I/O pair must be held in the same state, i.e., both at VCCI or both at GND.请问这个有必要吗?我觉得没有用到的悬空就行了,为什么还要接成固定电平?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TXB0108
请问TXB0108的datasheet上说没有用到的IO要接GND或电源,如下:The A and B sides of an unused data I/O pair must be held in the same state, i.e., both at VCCI or both at GND.请问这个有必要吗?我觉得没有用到的悬空就行了,为什么还要接成固定电平?
但是这个芯片的8个数据通道应该是独立的,其中的一个通道不用的话(悬空),即便它不稳定,我觉得也不会对其他数据通道造成影响,而且这个芯片的功耗本来就微乎其微,完全可以忽略的,请问能不能反驳一下?
一般情况下,芯片不带有总线保持功能(Bus Hold)的,不用的IO都需要拉高或拉低,除了避免额外功耗之外,也防止无效的输入电平或者无源驱动时使其保持在一个有效的逻辑电平,参考如下应用文档的介绍:
但是这个芯片的8个数据通道应该是独立的,其中的一个通道不用的话(悬空),即便它不稳定,我觉得也不会对其他数据通道造成影响,而且这个芯片的功耗本来就微乎其微,完全可以忽略的,请问能不能反驳一下?
8个通道是相互独立的,你可以参考下上面提供的应用手册,我们看到输入级的架构,是由一个 PMOS和一个NMOS构成,如果不给输入端一个固定的逻辑高或逻辑低电平的话,如果有无效的输入状态,那么PMOS和NMOS都有可能在其阈值之内,使得两个管子同时导通,这样就会从VCC到GND突然有个电流产生,很有可能会对芯片造成损坏。所以是不建议直接悬空的。