This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CD4066Bx导通电压的问题~

实验目的:用CD4066Bx来分离信号

实验现象:1、CD4066BM(贴片封装)工作在VDD=3.3V;VSS=GND,单片机PWM(电压3.2V)输出驱动CD4066开关引脚,用示波器测试CD4066BM输出端:结果在3.3V和5V工作电压下均无信号输出。

2、CD4066BE(直插封装)工作在VDD=5V;VSS=GND,单片机PWM(电压3.2V)输出驱动CD4066开关引脚,同样的测试方法,用示波器测试,信号成功分离。

问题:1、贴片封装的CD4066导通电压要比直插封装的高吗?

2、CD4066工作在VDD=3.3V;VSS=GND条件下的导通电压是多少?datasheet说明5V时,导通电压为3.5V

3、如果单片机的TLL输出高于VIH,直接用单片机的TTL输出驱动CD4066合理吗?

谢谢~!