This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助FPGA与DB9的控制线相连接的电平转换芯片

您好,

我想把DB9的控制引脚接到FPGA上,以方便更多应用。然而FPGA的控制线电平好像是-3到-15V为0,3到15V为1,在-3到3V是一个无意义的状态。是否是这样?请问有什么芯片能够做电平转换,方便我的使用?

谢谢

  • DB9即RS-232的接口你为何要直接到fpga,另外一边你用的什么控制? 如果是调试接口请用JTAG.  

    FPGA的接口逻辑电平也是根据FPGA型号定义的.要做逻辑电平转换之前请弄明白你是要什么电平转什么电平, 相关资料请看TXB0106系列,谢谢

  • 如果3到-15V为逻辑0,3到15V为逻辑1的话,那么-3~3V便是高阻抗状态,这样的电平转换器件,可以先做升压处理。