想请教下TI的工程师,MCU->DS90UB927Q->DS90UB928Q的架构中,928和927只有LVDS通道上的连接,928的IIC硬件接口是不直连到MCU的,也就是928和MCU的通信通道为928 LVDS->927->MCU这样,MCU可以通过LVDS的通道对DS90UB928Q进行寄存器设置吗?如果可以,在初始化时,927和928的LVDS通道都默认为I2C直连通道?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想请教下TI的工程师,MCU->DS90UB927Q->DS90UB928Q的架构中,928和927只有LVDS通道上的连接,928的IIC硬件接口是不直连到MCU的,也就是928和MCU的通信通道为928 LVDS->927->MCU这样,MCU可以通过LVDS的通道对DS90UB928Q进行寄存器设置吗?如果可以,在初始化时,927和928的LVDS通道都默认为I2C直连通道?
想请教下,LVDS可以传输的信号种类有哪些?
产品的调光信号PWM能不能也从LVDS传输?如果可以是同时传输还是分时传输?
传输视频信号的同时,I2C的通信是怎么传输的?同时的吗?还是分时传输。
LVDS是差分信号,不能传输PWM信号。I2C 是串行控制接口,可通过I2C接口对其进行寄存器的配置,并不是通过I2C传输视频信号。
我们的设想是通过 MCU-925-928的一个通道,MCU直接对928的GPIO口进行操作产生PWM信号,这样是可行的吗?
预想中:MCU对928的GPIO操作产生PWM时,其它操作是不可能进行的?因为通信通道被占用了,这样理解没错吧?
我们的LVDS通道上的数据有:I2C控制信号,视频信号,触摸屏的中断及RESET信号
按你们经验,这样的方案是可行的吗?
方案构架:MCU+925+928+LCD+TP(触摸屏)
方案描述:1、视频信号同925和928的LVDS通道完成传输,输送到LCD
2、TP数据由I2C通道接到928,然后通过928的LVDS通道和MCU通信
3、TP RESET、背光的PWM信号、背光的电源开关控制信号连接到928的GPIO,由MCU对928 的GPIO操作,完成这些信号的控制
4、TP的中断信号通过928的中断PIN输入,925的中断PIN输出,传送到MCU,完成TP的中断响应
能不能帮忙评估下以上方案的可行性,或者有什么漏洞。
再次麻烦您了,谢谢!
祝工作愉快