我现在有三路输入的DVI信号,想转成4路VGA输出,就是这4路VGA可以任意切换他的输入源(3选1),并且支持vga的输入源可以是同一个dvi信号。
我现在想的是 先把dvi信号变成rgb信号,比如用芯片adv7611,然后进入fpga,进行多路选择切换,然后用视频da把信号转成vga。不知道还有没有更好的解决办法?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DVI 和RGB 信号扇出芯片都没有,如果是输出3路RGB的话就好办了,直接采用TMDS361B进行DVI的3选1,然后经过TFP401进行TMDS到 RGB信号的转换。
TFP401这个芯片我看了是输出有奇数像素和偶像素,两种模式都用到这两个输出,一种是同时都有,一种是序列(即交替)。
由于后面的FPGA管教有限,但是又不想损失图像质量(图像看起来不能失真),可以只用其中一路接到我的FPGA上么?
如果可以的话,该怎么配置?请大概讲讲,谢谢