Other Parts Discussed in Thread: RCV420
TI技术支持您好:
我想用TI的4-20MA 转0-5V芯片RCV420,该芯片使用正负15V双电源,我想知道这个芯片需要正负15V电源提供多大的电流才能正常工作?数据手册中给出了,当输出额定电压为EO=10V时,输出额定电流最小为+10MA到-5MA,这个数值是最小额定电流,手册中没有给出最大电流,我使用DC-DC电源模块,输入24V,输出正负15V,该电源模块最大输出电流正负33MA,最小输出电流正负4MA,能满足RCV420的供电要求吗?另外,通常4-20MA这种电流传输形式,当传输电流小于4MA,可以认为断线了,要报警,但是芯片输出为0-5V,电流为0时,输出电压为多少才认为是断线,需要报警呢?希望您能尽快回付,非常感谢您的帮助!!!!