This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTD3384和SN74LVC541AW区别

Other Parts Discussed in Thread: SN74CBTD3384, MAX232, SN74LVC541A

我看见别人的电路图上DSP2812和max232芯片连接时,中间接了个SN74CBTD3384芯片,是不是进行电平转换的?能不能用SN74LVC541AW代替?

  • Hi Yuan,

    SN74CBTD3384 是 高速总线开关,可以实现电平转换,SN74LVC541A是低电压CMOS驱动器件,两者功能完全不同。所以,如果需要电平转换,则不能采用SN74LVC541替代CBTD3384器件。

    best regards,

    Steven

  • 我就想知道将F2812和MAX232中间的74CBTD3384换成74SNLVC541行吗?541的作用不就是将输入的低于0.8V的电平转换成0.4V的低电平,将高于2V的电平转换成3~3.3的高电平输出吗?这不也就是为了解决TTL电平和CMOS电平器件连接时的电平匹配问题吗,我认为541起的就是电平转换功能,和74CBTD3384在这里起的作用不是一样的吗?

  • Yuan,

    你说的没错, SN74LVC541可以将输入的低于0.8V的电平转换成0.4V左右的低电平,将高于2V的电平转换成3~3.3的高电平输出。

    可以把你提及到的电路原理图发到pw@ti.com吗?

    最简单的方法是直接使用支持较低电平接口的RS-232收发芯片, 有机会不需要增加额外的电平转换芯片。

    Best regards,

    Pony Wang

  • Yuan,你好

    SN74CBTD3384芯片主要用于总线开关,避免众多的器件干扰总线,电平转换只是他的附加功能。从这个角度上讲,SN74LVC541AW代替它不是一个好的选择。