This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB940-Q1: UB940与UB927配对

Part Number: DS90UB940-Q1

Hi,请问UB940接UB927时,940这边需要如何设置,UB927部分客户已经接928+显示屏验证可以正常显示是720p 30帧率。

UB940硬件是接的RIN0输入,CSI0输出 4 data lanes,配置脚MODE0和MODE1拉低。

UB940软件配置是 0x6b寄存器写0x40,OFMT=YUV420,IFMT=RGB444,处理器捕捉的mipi csi图像是1270*360,Y方向被压缩了一半。

如果0x6b寄存器写0x50,OFMT=YUV422,IFMT=RGB444,处理器捕捉的mipi csi图像是1270*16,Y方向被压缩的更多。

然而我的处理器mipi csi驱动配置的是yuv422格式 UYVY8_2X8。

下面是UB940和UB927的寄存器值:

x 出现错误。请重试或与管理员联系。