Other Parts Discussed in Thread: LMX2581, PLLATINUMSIM-SW
谁能告诉一下LMX2581内部4个VCO每个的具体频段吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
四个vco交叠覆盖了1850 - 3760M的频段, 每个vco有分了256个频带进行校准, 将会自动校准选择VCO. 实际应用中不必知道各个VCO频点,将自动选择,谢谢.
Dear Robin Feng:
您好。我目前正在测试LMX2581,也希望测试其手动控制VCO频率分段,能否将LMX2581的4个VCO频率划分资料发给我吗?
另外,能给我一些关于手动换频的建议吗?如:R15 .R3.R1.R0 的送数顺序和其他注意事项。
邮件请发:victory5@163.com.
谢谢!
您好:
目前我使用LMX2581产生宽带本振载波,4个VCO都会使用,发现当使用参考和PFD都为10M时,2200uA,100k环路,测试芯片的LD引脚电平突变间距,锁定时间130-200us,让当使用参考和PFD都为100M时,测试锁定时间30-60us。我通过PLLatinum软件的推荐code值拟合4个VCO的计算曲线,还算线性,例如3G为VCO3的106,但是对减小锁定时间的帮助不大,改变环路有些影响,但是不稳定有好有坏,甚是烦恼。
请问该芯片的VCO的子段划分?找到正确的code后数字校准时间真能减小?器件资料中的10us如何能实现?只有提高PFD频率?
希望您能指导我完成锁定时间问题的解决,急求支持!谢谢!
您可以通过PLLatinum 仿真工具进行仿真。链接如下:http://www.ti.com.cn/tool/cn/pllatinumsim-sw
你好:参看我另外一贴,一般条件下提高锁定时间方法如下。不知道你设置是否正确?
1.预选VCO; 由于LMX2581是宽带器件,内置了4个VCO以覆盖所有频段,因此通过VCO_SEL预选vco可以减小锁定时间;
2.使用快锁,并在寄存器做相应配置,Engages Fastlock;
3.环路设置,环路带宽越宽的话锁定时间会越快;