Other Parts Discussed in Thread: LMK04803
我用 信号分析仪 测量输出时钟,测得的数据,其单位是dbm。
LMK04803的DATASHEET上,给出的单位是dbc/Hz。
dbm与dbc/Hz之间,是如何换算的呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi James,
The dBm and dBc are completely different so there is no 'conversion' between the two.
dBm - indicates the power measurement relative to 1 milliwatt. 0 dBm means no change from 1 mW, i.e. a power of exactly 1 mW. 3 dBm means 3 dB greater than 0 dBm. dBm is the relative difference to a fixed reference power of 1 mW.
dBc — indicates the power relative to the power of the main carrier frequency; typically used to describe spurs, noise, channel crosstalk, and intermodal signals which may interfere with the carrier. dBc is the relative difference to an arbitrary reference power level, the power level of the carrier frequency.