您好!我想请问下,TI哪种型号的电压电平转换芯片适合用于I2S信号从1.2V到1.8V的电平转换?请问TXS0304或TXB0304芯片是否满足上述要求?请问是否有TXS0304的说明书?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,TI有很多转1.2到1.8的芯片。请问您的I2S的传输速率是多少?输入信号是Push-pull的 还是open-drain的?
如果是Push-pull的话 建议用TXB的产品。如果是Open-drain的,建议用TXS产品。欢迎使用。
我理解下来,IIS接口应该是push pull的,所以建议用TXB0304,一般来说IIS的时钟速率不会超过24MHz,所以TXB0304应该没有什么问题。