请问TI工程师,对928的LVDS信号的眼图有什么评价要求?有没相关的性能要求文档?
在实用中用泰克TDSP3500测试,USB2.0眼图评价波形如下,这是不OK的。有什么推荐的测试方法没,盼回复
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个是你测试928的LVDS差分对的眼图,为什么写的是USB2.0的眼图? 测试的时候,有没有外接100ohm终端匹配电阻?
谢谢你的关注,因为没有专门的分析仪,我测的时候用的是泰克的示波器,利用过滤器自带的USB2.0信号分析功能,里面有眼图及抖动的分析。
另外,测试的时候是带实际负载的,是一块LVDS接口的LCD屏,因此没有接100ohm的电阻。有试过加电阻,LVDS信号幅值会下降100mv左右
泰克示波器可以测得,但是不能用分析USB信号的程式来分析LVDS的眼图。 你可以直接采用差分探棒测试LVDS的差分对,如果示波器测得的单笔数据不好分析的话,可以做累积,然后分析眼图。
这里有一份关于FPD link II and III CML output test application note share to you.